AXIS#.DBILIMIT
Description
This parameter sets the maximum amplitude of the current for dynamic braking. AXIS#.DBILIMIT can only be set manually when AXIS#.MOTOR.DISAUTOSET index (28) is set to 1. Setting AXIS#.MOTOR.AUTOSET to 0 does not make AXIS#.DBILIMIT writeable.
-
- If the motor or drive current is in foldback before entering dynamic brake mode, the actual current limit might be less than AXIS#.DBILIMIT when dynamic braking starts. The current will be limited to the minimum of AXIS#.DBILIMIT and AXIS#.IL.IFOLD . Once the foldback current recovers, AXIS#.DBILIMIT will be the enforced current limit.
Example
Setting AXIS#.DBILIMIT to 2 limits the dynamic brake current to 2 Arms.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 | |
| Bug fix | 02-08-00-000 | The bug caused AXIS#.DBILIMIT to be reset to its default value under some conditions. The fix involved making the parameter read only by default and calculated from motor parameters. |
General Information
|
Type |
Read/Write |
|
Units |
Arms |
|
Range |
0 to minimum of drive peak current (IPEAK) and motor peak current (AXIS#.MOTOR.IPEAK ). |
|
Default Value |
Drive continuous current (ICONT) |
|
Data Type |
Float |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.DBILIMIT | 0x5000 | 0x7 | UDINT | 1000:1 | - | RW | False |
| AXIS2.DBILIMIT | 0x5100 | 0x7 | UDINT | 1000:1 | - | RW | False |